DOCA0214EN–06

Insulating Screen

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • It is mandatory to install insulating screens or custom made fiber insulating plates when clearance distance of wiring is less than the minimum clearance distance.
Failure to follow these instructions will result in death or serious injury.

Insulating screens are installed at the front or rear of the power terminals of the transfer switching equipment to provide insulation between phases.

The table below provides the list of insulating screens:

Switch

Insulating screen

Frame 250: 100–250 A

TPSISO66

Frame 630: 320–630 A

Frame 800: 800 A

TPSISO67

For information on installation, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601

  • TransferPacT Active Automatic / Automatic / Remote 800 A: BQT1751501

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?