DOCA0214EN–06

Overview

The RTSE transfers to a stable position after receiving a rising edge signal. The rising edge signal should last for no less than 200 ms.

The RTSE will remain on the stable position until receiving a new signal. It will not respond to the new signal when:

  • Position slider is in the left and transfer switch equipment is in RUN mode.

  • Transfer switch equipment is in alarm state.

  • Transfer switch equipment is executing the transfer action.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?