DOCA0214EN–06

Fire Protection Dry Contact Input

The fire protection is an accessory module installed on TransferPacT Automatic and TransferPacT Active Automatic controller with following functions:

  • Exit the auto transfer mode and transfer the switch to OFF according to input signal.

  • Fire protection with 1 dry contact input.

  • Green LED on the front face of the accessory indicates the power status and proper connection of the accessory.

  • The main MCU on ATSE communication through CAN bus.

  • Only one module is allowed to be installed on one product.

Application

When there is fire emergency, the fire protection signal can transfer ATSE to off position.

Terminals

  • Fire protection with 1 dry contact input:

    • W1.W2

Performance

Electrical Characteristics

Ratings

Ui

30 Vdc

Minimum input current

5 mA

Altitude

2000 m

Cable Capacity for Terminals

The cable capacity for the terminals are 0.05 – 2.6 mm2 (AWG 30 ~ 13).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?