DOCA0214EN–06

Utility-Utility Operation

  1. Detect the normal source contingency (Utility).
  2. Transfer the load to replace alternate source (Utility) when normal source is out of tolerance.
  3. Re-transfer to normal source when it is recovered if auto return mode is set.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?