DOCA0214EN–06

Position Indicator

TransferPacT Active Automatic / Automatic 32-100, 80-160, 100-250, 320-630, 800 A
TransferPacT Remote 160-250, 320-630, 800 A

Position indicator

Status

OFF

Source I is connected

Source II is connected

TransferPacT Active Automatic 800-1600 A

Position indicator

Status

Device is OFF, and mechanism spring is charged.

Device is OFF, and mechanism spring is discharged.

Source I is connected, and mechanism spring is charged.

Source I is connected, and mechanism spring is discharged.

Source II is connected, and mechanism spring is charged.

Source II is connected, and mechanism spring is discharged.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?