Terminal Extension
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
The terminal extensions are used to extend the connection possibilities of the switch.
The terminal extensions are screwed on the switch using the screws delivered with the terminal extensions.
The table below provides the list of the straight terminal extension:
|
Switch |
Number of poles |
Straight terminal extensions |
|---|---|---|
|
Frame 250: 100–250 A |
3P |
LV429263 |
|
4P |
LV429264 |
The table below provides the list of the edgewise terminal extension:
|
Switch |
Number of poles |
Edgewise terminal extensions |
|---|---|---|
|
Frame 250: 100–250 A |
3P |
LV429308 |
|
4P |
LV429309 |
|
|
Frame 630: 320–630 A |
3P |
TPSCON55 |
|
4P |
TPSCON56 |
For information on installation, consult the instruction sheets on Schneider Electric website:
-
TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501
-
TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601
DANGER