Event Logs
TransferPacT ATSE can record maximum up to 99 events of the event logs. If it exceeds the events limit, the latest logs will overwrite the previous event logs. The limit of event logs on LCD and Modbus are:
-
LCD can only display the last 20 events.
-
Modbus can display all the events.
Perform the following procedure to check the event logs:
-
Select the Status page from Home page and press OK button.
-
Select Event Logs option and press OK button.
-
Select SI Back To Normal.
-
Press OK button to check the selected event log.
Event Logs Page Description
|
Label |
Description |
|---|---|
|
1 |
Time of events.
NOTE: Without any time
calibration or external DC 24 V, after long terms shut down of controller,
the timer may show wrong.
|
|
2 |
The source status during the events. |
|
3 |
Code of events. |
|
4 |
Transfer mode during the events. |
List of Event Logs
|
Event Code |
LCD Display |
|---|---|
|
1 |
Position alarm: Transfer to A Failed |
|
2 |
Position alarm: Transfer to N Failed |
|
3 |
Position alarm: Transfer to OFF Failed |
|
4 |
Position alarm: Transfer to Invalid Position |
|
5 |
Position Alarm: Internal Error |
|
6 |
Position alarm: Unexpected position |
|
10 |
SI Phase Rotation Error |
|
11 |
SII Phase Rotation Error |
|
12 |
Unsupported Device RS Alarm |
|
30 |
Genset Invalid |
|
31 |
Genset Start Failure |
|
40 |
On Load Test Failure |
|
41 |
Off Load Test Failure |
|
42 |
On Load Test Success |
|
43 |
Off Load Test Success |
|
50 |
SI Unbalance Warning |
|
51 |
SII Unbalance Warning |
|
52 |
SI Neutral Position Wrong Warning |
|
53 |
SII Neutral Position Wrong Warning |
|
54 |
SI Neutral Loss Warning |
|
55 |
SII Neutral Loss Warning |
|
70 |
SI Undervoltage |
|
71 |
SII Undervoltage |
|
72 |
SI Overvoltage |
|
73 |
SII Overvoltage |
|
74 |
SI No Voltage |
|
75 |
SII No Voltage |
|
76 |
SI Underfrequency |
|
77 |
SII Underfrequency |
|
78 |
SI Overfrequency |
|
79 |
SII Overfrequency |
|
80 |
SI All Recover |
|
81 |
SII All Recover |
|
100 |
SI Voltage over 500 V |
|
101 |
SII Voltage over 500 V |
|
120 |
Transfer from N to A |
|
121 |
Transfer from A to N |
|
122 |
Transfer from N to O |
|
123 |
Transfer from A to O |
|
124 |
Transfer from O to N |
|
125 |
Transfer from O to A |
|
140 |
Load Shedding Output |
|
141 |
Genset Start |
|
142 |
Genset Stop |
|
143 |
Alarm Output Start |
|
144 |
Alarm Output Stop |
|
145 |
Force to OFF |
|
146 |
Fire Start |
|
147 |
Fire Stop |
|
148 |
Enter Inhibit Mode |
|
149 |
On Load Test |
|
150 |
Off Load Test |
|
151 |
Voluntary to N |
|
152 |
Voluntary to A |
|
153 |
Comm Transfer Exit |
|
154 |
Comm Transfer to N |
|
155 |
Comm Transfer to A |
|
156 |
Comm Transfer to OFF |
|
200 |
Operation Mode Changed |