DOCA0214EN–06

Wiring Diagram for Source Position Auxiliary Contacts

TPSAUX32/ TPSAUX43/ TPSAUX71 (Installed on left side)

ATSE is closed at SI:

  • F11-F14 is closed

  • F11-F12 is opened

ATSE is closed at SII:

  • F21-F24 is closed

  • F21-F22 is opened

ATSE is at OFF position:

  • F11-F12 and F21-F22 are closed

  • F11-F14 and F21-F24 are opened

TPSAUX71 (Installed on right side)

ATSE is closed at SI:

  • F21-F24 is closed

  • F21-F22 is opened

ATSE is closed at SII:

  • F11-F14 is closed

  • F11-F12 is opened

ATSE is at OFF position:

  • F21-F22 and F11-F12 are closed

  • F21-F24 and F11-F14 are opened

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?