Transfer Inhibit and Remote Testing
The transfer inhibit and remote testing is an accessory module installed on TransferPacT Automatic and TransferPacT Active Automatic controller with following functions:
-
Transfer inhibit, 1 NO dry contact is provided.
-
Remote testing, 1 NO dry contact is provided.
-
Green LED on the top of the accessory indicates the power status and proper connection of the accessory.
-
Communication with the main MCU on ATSE.
-
Only one transfer inhibit and remote testing module is allowed to be installed on each TSE.
Application Transfer Inhibit
-
Transfer Inhibit when there is power interruption because of short circuit.
-
This function can be used to lock the controller by customized signals.
-
This function can be used for cooperation with different ATSE.
-
Remove transfer inhibit signal to exit this mode.
Application Remote Testing
-
Remote testing is an input signal to start test procedure.
-
The remote test can only be started at Auto mode.
-
For Active Automatic HMI, on load test, off load test and time duration can be selected.
-
For Automatic HMI, on load test is unlimited. Stop the test manually by opening the dielectric switch on ATSE, and it should be back in run position to resume the controller function.
Terminals
For transfer inhibit: 1 input
-
Inputs : TI1-TI2
For remote testing: 1 input
-
Inputs : RT1-RT2
Signal Type
-
Digital input with dry contact
-
Need over 200 ms input to start transfer inhibit and remote test
Performance
|
Electrical characteristics |
Ratings |
|---|---|
|
Ui |
30 V DC |
|
Maximum Input current |
5 mA |
|
Altitude |
2000 m |
Cable Capacity for Terminals
The cable capacity for the terminals are 0.05 – 2.6 mm2 (AWG 30 ~ 13).