Cable-lug Adapter
Cable-lug adapters are used to adapt the cable lug connection on vertical connection adapters of the TransferPacT Active Automatic 800–1600 A Transfer switching equipment.
Cable-lug adapters are screwed on the switch using the screws delivered with the cable-lug adapters.
The table below provides the list of the vertical connection adapter:
|
Switch |
Number of poles |
Vertical connection adapter |
|---|---|---|
|
Frame 1600: 800–1600 A |
3P |
33644 / LV833644SP |
|
4P |
33645 / LV833645SP |
For information on installation, consult the instruction sheet on the Schneider Electric website: BQT7680301 .