DOCA0214EN–06

Overview

TransferPacT Remote provides transfer solutions with input and output terminals.

The details of the input and output terminals are shown below:

Terminals

Marking

Definition

Product Availability

P0

Common terminal for P1, P2

P1

Output signal, when either source voltage is in range and product is NOT in manual mode, NO terminal will close.

P2

Output signal, when either source voltage is in range and product is NOT in manual mode, NC terminal will open.

Remote Transfer

R0

Common terminal for R1, R2, R3

R1

Passive input signal, remote transfer to position I when closed with R0 and last for at least 200 ms.

R2

Passive input signal, remote transfer to position II when closed with R0 and last for at least 200 ms.

R3

Passive input signal, remote transfer to position O when closed with R0 and last for at least 200 ms.

For information on installation of input and output terminals, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601

  • TransferPacT Active Automatic / Automatic / Remote 800 A: BQT1751501

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?