DOCA0214EN–06

Preferable Source Selection

TransferPacT Active Automatic provide an easy way to select the preferred source as normal source.

When the genset is at normal power and the utility is not so stable, make the selection as below:

For TransferPacT Active Automatic: To select the preferred source, go to Source Configuration page to make the selection.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?