DOCA0214EN–06

Steel Connector

CAUTION
Hazard of overheating
Do not use steel connectors LV429242 or LV429243 over 160 A.
Failure to follow these instructions can result in injury or equipment damage.

Steel connectors can be used to connect the switch and power cables.

They can be mounted on the TransferPacT Active Automatic / Automatic / Remote 100-250 A transfer switching equipment.

The table below provides the list of steel connectors.

Switch Number of poles Steel connectors

Frame 250: 100–250 A

3P

LV429242

4P

LV429243

For information on installation, consult the instruction sheet on Schneider Electric website: GEX2525501.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?