Equipment Description
|
Label |
Description |
|---|---|
|
A |
Position for HMI modular |
|
B |
Active Automatic HMI (with LCD display) |
|
C |
Automatic HMI (with rotary switch) |
|
D |
Slots for function module |
|
E |
Power connections |
|
F |
Position indicator |
|
G |
3- position slider: Auto/Manual/Lock |
|
H |
Single line diagram |
|
I |
Dielectric switch |
|
J |
Protective earth |
|
K |
Carrying grip |
|
L |
Spring charged and ready-to-open indicator |
|
M |
Spring charged handle |
|
N |
Source II push button |
|
O |
OFF position push button |
|
P |
Source I push button |
|
Q |
Mounting side plate |