DOCA0214EN–06

Neutral Loss

Field

Description

Applications

  • A warning is raised when this function is enabled to prevent wrong connection, miss connection or disconnection caused by interior or exterior impacts of neutral cable.

  • Only available for TransferPacT Active Automatic.

Default value

This feature could be enabled or disabled. By default, it is disabled.

The LED of source will blink to warn when there is neutral loss after the sensor is enabled.

Detection criteria

When the load is connected to the power source and live, the unbalanced loads are detected.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?