Compression Lug
DANGER |
|---|
|
hazard of electric shock, explosion or arc flash
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
Hazard of fire
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The compression lugs are screwed on the switch using the screws delivered with the switch.
The table below provides the list of the compression lugs:
|
Switch |
Number of poles |
Material |
Compression lug |
|---|---|---|---|
|
Frame 250 : 100–250 A |
3P |
Cu |
LV429252 |
|
LV429253 |
|||
|
LV429254 |
|||
|
Al |
LV429504 |
||
|
LV429506 |
|||
|
4P |
Cu |
LV429256 |
|
|
LV429257 |
|||
|
LV429258 |
|||
|
Al |
LV429505 |
||
|
LV429507 |
|||
|
Frame 630: 320–630 A |
3P |
Cu |
TPSCON57 |
|
TPSCON59 |
|||
|
Al |
TPSCON61 |
||
|
TPSCON63 |
|||
|
4P |
Cu |
TPSCON58 |
|
|
TPSCON60 |
|||
|
Al |
TPSCON62 |
||
|
TPSCON64 |
|||
|
Frame 800: 800 A |
3P |
Cu |
TPSCON57 |
|
TPSCON59 |
|||
|
4P |
Cu |
TPSCON58 |
|
|
TPSCON60 |
For information on installation, consult the instruction sheets on Schneider Electric website:
-
TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501
-
TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601
-
TransferPacT Active Automatic / Automatic / Remote 800 A: BQT1751501
DANGER
WARNING