DOCA0214EN–06

Force to Off Mode

  • Transfer ATSE to OFF position with an emergency stop order. All the other transfer mode will be canceled except handle control. There should be no time delay.

  • Exit Force after signal disappeared.

  • Accessories are required using TPCDIO07 to extend this function of TSE.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?