DOCA0214EN–06

Transfer Condition

The following are the auto-transfer conditions:

  • Voltage deviation: Controller monitors two sources, and uses over-voltages and under-voltages thresholds as conditions of source transfer.

  • Frequency deviation: Controller monitors two sources, and uses over-frequency and under-frequency thresholds as conditions of source transfer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?