Add to Selection

When using the ArcFM Locator tool (accessed with the ArcFM Locator tool button on the ArcFM toolbar), you can add the search results to the Attribute Editor Selection tab. Add to Selection is available when you right-click a single feature or multiple features.

  1. There are two ways to add located features to your Selection tab.
    • Before clicking the Find button, you can select the Auto Add to Selection checkbox. Designer will add all items it located in the search to the Selection tab.

    • After Designer performs the search, you can right-click the features or layer listed in the results window and select Add to Selection.

  2. Designer lists the feature on the Selection tab of the Attribute Editor.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.