Design Optimization
Design Optimization simplifies the design process by using pre-defined parameters (set by your administrator) to automatically place the optimal features for your layout. Your administrator can elect to provide multiple design type parameters. You can tailor each set of parameters toward a specific type of design. Design Optimization includes default symbology for Front Lot Electric URD designs. Review the Design Optimization Default Symbology section for more details.
To use Design Optimization, you must have a design open. The Design
            Optimization button will not enable without an open design. With a
            design open, click the Design Optimization  button
            on the Designer toolbar to launch the Design Optimization window.
 button
            on the Designer toolbar to launch the Design Optimization window.
This window displays the tasks that must be performed to optimize your design. Click any of the green icons to view the associated task parameters. You cannot perform tasks with a red octagon icon until previous tasks are complete.
Before you Begin: Ensure your data does not contain overlapping parcels or gaps between property lines. These two data cases will cause errors in Design Optimization.