Designer Utility Tools

Right-click a feature in the Attribute Editor to access Designer utility tools. Select Zoom To, Highlight, Quick Attribute Viewer, Delete, Remove from Selection, Send to Targets, Send to Design, Copy, Remove from Selection, Update Work Flow Status, or Feeder Manager Translator. When you right-click related objects, Unrelate Object is also an option.

The utility tool in blue text (Zoom To in the example above) indicates the default action. The default is the first option and occurs when you double-click a feature.

When using the Locator tool you can also select the Add to Selection utility by right-clicking a feature in the Locator results listing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.