Create a New Map Set

A map set is a collection of map elements, stored display, and printing options that can be saved and referenced when plotting maps. You may add a map set to an existing map book or create a new map book in which to add the new map set.

  1. In the Map Book Editor, right-click a map book and select Create Map Set.

  2. Enter a Title and Description, and click Apply to save changes.

  3. Click the Map Book Editor's Options tab to set the map set's display and scale settings.

     

    IMPORTANT: If a user adds a large number (i.e., 10,000 or more) of map grids to a map set, Map Production's performance will be slowed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.