View Device Catalogs

The catalogs provide material and electrical information for the load profile as well as the features. Catalogs cannot be edited at design time. By default, sample catalogs are provided for the following: Transformer, Pedestal, Secondary Conductor, and Service Conductor.

View the contents of the catalog by clicking on the catalog's tabbed pane and then clicking in the adjacent field and on the resulting Browse button as shown in the following example:

The associated Catalog Editor window appears after you click the browse button. You cannot edit the selected feature's information. Edit the MMENG_LOADPROFILES table (see ArcFM Solution Configuration Guide) to properly modify these features or add or delete members.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.