Graphic Favorite Categories

Much like System Favorite categories in ArcCatalog, these allow you to organize graphic favorites. On the Graphics list, categories are indicated with bars at the top and bottom of the list. Click a bar to view its contents. In the example below, the Devices category is displayed. You must have an edit session started to access the right-click tools that allow you to create, edit, and delete graphic favorite categories.

Create Category

  1. Right-click the Graphics list and select Create Favorite Category.
  2. Type a category name and click OK.

Edit Category Name

  1. Select an existing category to display its contents.
  2. Right-click within the category and select Edit Category Name.
  3. Type a new category name and click OK.

Move Category

  1. Start an Edit session.
  2. Click the title bar of a category.
  3. Drag and drop it to another position.

Delete Category

  1. Select an existing category to display its contents.
  2. Right-click within the category and select Delete Favorite Category.
  3. A confirmation screen will verify that you want to delete the selected category. Click Yes to delete or No to exit without deleting.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.