Map Production Options

The Map Production tab allows you to designate a default path for map files exported and printed to file from Map Production. If you do not indicate a default path, Map Production will use the last path used for a Map Production export (or print to file functionality).

To designate a default, select the Default Path radio button and enter a path. You may click the Browse button to browse to a location. All map files exported or printed to file from Map Production will be saved to the path entered. To use the last path, select the Use Last Path radio button.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.