Place Template Favorite Overview

Template Favorites allow you to easily place a select configuration of features or Designer-only compatible units (CUs). Depending on how the template favorite is designed, you can place points, spans, or choose from a given set of features (or CUs).

For example, a template favorite may allow you to place all of the features required for new residential service. This section describes how to place a template favorite on the map. During placement, ArcFM may prompt the user to edit attributes, select a feature from a choice list, select a CU (Designer only), or add a non-GIS CU (Designer only).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.