Edit Template Favorite

You can edit a favorite once it has been created on the Features list or CUs list.

  1. Right-click the template favorite and select Edit Template Favorite.

  2. Make changes in the Edit Template Favorite window. You can add points, add spans, add choice lists, or edit feature or compatible unit (CU) attributes.
  3. To remove a feature, right-click the feature or CU and select Remove.
  4. Use the up and down arrows to change the order of the features in the template favorite. ArcFM places features in the order they appear.
  5. Click Apply to accept edits.
  6. Click OK to save your changes and dismiss the Edit Template Favorite dialog.
  7. Click Cancel to dismiss the Edit Template Favorite dialog without saving your changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.