Edit Session

Available in: ArcFM Viewer for ArcGIS Engine (Inspector extension), ArcFM

Enable: Redline session open in ArcFM Viewer for ArcGIS Engine or ArcFM

This task allows a user to convert a redline session to an edit session. For example, a field inspector may create a redline session in the field, add graphics, then find the need to inspect a transformer. He need only execute the Edit Session task to convert the redline session to an edit session and perform the inspection.

This task is available only with the Inspector extension (field or enterprise) or with ArcFM.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.