Highlight

You can use the Highlight utility to see a selected feature or layer highlighted (the feature flashes three times) on the map. Use the General tab in ArcFM Options to modify the size and color of the Highlight.

  1. Right-click a feature or a layer on the Selection tab or QA/QC tab of the Attribute Editor to display the Utilities menu. This utility is also available in the Locator tool.

  2. Select Highlight, and you will see the features flash three times on the map. If the selected features are out of visible range, use Zoom To before using Highlight.
    TIP: If the highlighted features are hidden behind a form such as the Attribute Editor or Locator tool, the form window will become transparent to make the highlighted features visible when they flash.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.