Reverse Highlight

You can use the Reverse Highlight tool to quickly find one or more features in your Design tab tree based on features you select on the map. This tool is particularly useful when working with large designs.

  1. Select a design feature on the map.
  2. On Attribute Editor's Design tab, right-click anywhere on the design tree.
  3. Select Reverse Highlight.
  4. The tool automatically scrolls down the design tree list and expands necessary nodes to find the feature you have selected on the map.

    Select the feature on the map you want to find in the design tree.

    Once you click Reverse Highlight, the tool automatically finds the feature you selected.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.