Extension Licensing

ArcFM allows you to check out licenses for ArcFM extensions in ArcMap. It is no longer necessary to close ArcMap, open the ArcFM Desktop Administrator, then re-open ArcMap. This functionality allows you to check out a license on-the-fly.

IMPORTANT: Before turning on an extension, it needs to be installed as part of the ArcFM Solution installer. Scroll to the bottom of the Setup dialog when installing ArcFM Solution and locate Extensions. Expand the Extensions section to see the three extensions available to install; Conduit Manager, Network Adapter, and Redliner. Click the arrow next to each extension you want to select it for installation. Then continue with the install as normal.

  1. In ArcMap, select Customize > Extensions.

    TIP: Users will not need to check out an extension license for Network Adapter-DMS.

  2. Select the checkbox next to the license you want to use. If the license is not available (i.e., all licenses are in use or licenses were not purchased), then the extension license is labeled with: "License not available."

  3. Click Close to dismiss the Extensions window.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.