ArcFM Utility Tools

ArcFM utility tools let you navigate large map documents quickly by finding, highlighting, and moving features to the Targets or Selection tabs of the Attribute Editor. Access ArcFM utility tools by right-clicking a feature in the Attribute Editor and selecting an option. When using the Locator tool, you can send a feature to the Selection tab by right-clicking a feature in the Locator results list and selecting Add to Selection. Utility tools shown in blue are the default action. The default is the first option and the action that occurs when you double-click the feature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.