Remove Other Items from Selection

Use Remove Other Items From Selection to keep only the selected features and remove all other features listed in the Selection tab of the Attribute Editor. This tool can be helpful when selecting a large number of features. The tool does not delete features from the map.
  1. Select features in the Selection tab that you want to keep selected.
  2. Right-click any one of the selected features.
  3. Select Remove Other Items From Selection to remove all non-selected features.

  4. The Selection tab will update and show only the features you had selected. If you selected features from multiple layers, by default the remaining layers will display collapsed in the Selection tab. Layers will be removed from the Selection tab display if not features were selected within them before running the tool.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.