Conduit Tracing

The Conduit Manager trace task allows you to identify available ducts in your underground network. Conduit Tracing is available whether you have Conduit Manager licensed or not. Users may access Conduit Tracing tools from ArcFM and ArcFM Viewer. Also, you must select the network you created for conduit tracing in the Utility Network Analyst toolbar's Network field.

IMPORTANT: In order to perform a trace, the Enabled fields on the features in the geometric network must be set to True. Any feature with an Enabled value of False will be treated as a barrier in the trace. Existing features may be udpated using the Mass Attribute Update tool. For any future conduit system features, the default value for the Enabled field should be set to True, and the field hidden from the user through ArcFM properties. This ensures that all conduit features are always enabled for conduit tracing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.