Assign/Unassign/Complete

Publishes in Mobile config, Mobile tools, Desktop using, EXI

These buttons can be used to Assign, Unassign, or Complete markups. Logged-in users can assign markups to themselves that are either unassigned or assigned to another user. To assign a Markup to yourself, click Assign To Me.

To reassign a markup that is currently assigned to someone else, click Assign To Me. You are presented with a confirmation (Yes/No) choice to take ownership. If you select No, the markup remains assigned to its currently-assigned user. If you select Yes, the markup is reassigned.

Once assigned, a markup can be unassigned if it should be returned to the pool of available markups. Click Unassign. You cannot unassign markups that are not currently assigned to you.

The markup can also be completed by clicking Complete.

Once completed, select Yes or No.

If you select No, the markup remains assigned. If you select Yes, the following things happen:

  • The markup is removed from the list.

  • The markup features are removed from the map and the app.

  • A notification is sent to the app that markups have been closed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.