Conduit Trace Task
The Conduit Manager trace task allows you to identify available ducts in your underground network. The Conduit Manager Trace toolbar allows you to select the Conduit Manager trace as well as set the trace criteria. The trace tools will remain disabled until you have the underground geometric network selected. Use Esri's Utility Network Analyst toolbar to select a geometric network.
Conduit Manager Find Path
Trace: This trace allows you to identify available ducts given
various user-defined criteria. If multiple conduits (or ducts) exist
between two trace points (or manholes), the trace returns only the
first conduit found.
Clear Flags, Barriers, and
Results: This button removes all flags and barriers from the map.
It also clears the results if you have selected the Results as Drawings
option. If you choose to view your results as a selected set, the
Selection tab of the Attribute Editor will NOT be cleared.
Results as Selection: Use this toggle button to determine how the trace results are displayed.
When the button is depressed (or toggled on), the resulting features
are selected on the map and displayed on the Selection tab. When it
is toggled off, the resulting features are highlighted on the map
in red (you may change the default color using the Options button).
Zoom to Results: Use
this toggle button to elect whether to zoom to the trace results.
When this button is depressed (or toggled on), the map view will zoom
to the trace results.
Conduit Trace Criteria Setup: Click this button to modify the trace criteria. This dialog may also
be accessed through the Options button on the Conduit Manager Trace
toolbar.
Options: Click this button to set various options for your conduit trace.
Results tab
Select the format in which you'd like the results to be displayed. This option may also be set using the Results as Selection toggle button on the Conduit Manager Trace toolbar. Use the Results content field to indicate the features that should be included in the trace.
Conduit Traces tab
Click the Set Conduit Trace Criteria button to set trace criteria. Select the checkbox to generate a report after the trace.