Remove from Selection/Remove All from Selection

This tool allows you to remove features from the Selection Tab of the Attribute Editor. It does not delete features from the map.

  1. Right-click a feature listed on the Selection tab.
  2. Select Remove from Selection to remove only the selected features. Select Remove All from Selection to clear the Selection tab.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.