Quick Attribute Viewer

The Quick Attribute Viewer is a read-only display of feature attributes and values. You can display multiple Quick Attribute Viewer windows.

  1. Right-click a feature on the Selection tab of the Attribute Editor to display the Utilities menu.
  2. Select Quick Attribute Viewer to display.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.