Pan To

This right-click utility allows you to refocus the display to include the selected features without changing the scale. In the example below, the user chooses to Pan To when the scale is set at 1:550. Figure 2 shows that the display now includes the selected feature and the scale remains 1:550. You can use Pan To with multiple features. However, all of the selected features may not appear in the display if the scale doesn't allow.

In the following image, Pan To is selected at a scale of 1:550:

In the following image, the display includes the feature, and the scale remains 1:550:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.