Mode Selector

You can find the Mode Selector on the Designer toolbar.

  1. Open a design through the WMS to enable Mode Selector.
  2. Check Designer or ArcFM to switch modes.

    If the Mode Selector does not appear on your Designer toolbar, it may NOT be added like other tools. Instead, you will have to reset the toolbar. Right-click in the gray area around the toolbars and select customize. On the Toolbars tab, select the Designer toolbar and click the Reset button.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.