Designer Toolbar

The Designer toolbar accesses a collection of tools that increases productivity and functionality during ArcMap sessions. If the Designer toolbar is not displayed, click View > Toolbars, then check Designer on the dropdown list. Or you can right-click in the gray toolbar area and select Designer from the list. This toolbar is dockable.


: About ArcFM Solution

: Designer CU to WL Assignment

: Quick Estimate

: Cable Pulling Analysis

: Map Production in Designer

: Mode Selector

: Design Optimization

The following button does not appear on the toolbar by default and must be added using Tools > Customize.

: Secondary Circuit Analysis

  1. To add buttons to the toolbar:
    1. Right-click the gray area of the toolbar and select Customize.
    2. Select the Commands tab and click ArcFM Solution.
    3. Drag icons from Commands and drop on the toolbar.
  2. To remove buttons from the toolbar:
    1. Right-click the gray area of the toolbar and select Customize.
    2. Drag the button from the toolbar and drop it anywhere off the toolbar.
  3. To restore default buttons:
    1. Click the Toolbars tab.
    2. Highlight the toolbar you want to reset.
    3. Click Reset to restore any removed default buttons.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.