EIO0000004205.07

12-inch 和 15-inch

正视图
A. 前 USB 盖
B. USB 2.0 (A 型)*1
C. USB 2.0 (micro-B)(此接口不可用。)
D. 状态 LED

*1 默认情况下,前面 USB 被禁用。要启用,请在Launcher中设置。

反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.