DOCA0257ZH-CN-01

温度保护

描述

TeSys Tera system 支持以下温度输入:

  • LTMT main unit 上的一个温度输入,可配置为 PT100 或 PTC。

温度保护功能生成以下信号:

  • 报警:温度值高于报警级别。

  • 脱扣:在所需时间延迟内,温度值高于脱扣级别。

LTMT Main Unit 参数设置

LTMT main unit 的温度保护功能具有以下可配置的设置:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Disable

PT100 trip level (applicable if PT100 sensor is selected)

25.0–180.0 °C in step of 0.1 °C

130.0 °C

PTC trip level (applicable if PTC sensor is selected)

2700–4000 Ω in step of 1 Ω

2700 Ω

PTC trip level reset (if PTC sensor is selected)

1600–2300 Ω in step of 1 Ω

1600 Ω

Time Delay

0.1–6000.0 s in step of 0.1 s

1 s

PT100 alarm level (applicable if PT100 sensor is selected)

25.0–180.0 °C in step of 0.1 °C

130.0 °C

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.