DOCA0257ZH-CN-01

欠频

描述

Under Frequency 保护功能生成以下信号:

  • 报警:测得的频率低于报警级别。

  • 脱扣:在指定时间延迟内,测得的频率低于脱扣级别。

注: 在检测到电压后的 500 毫秒内,将启用此功能。

参数设置

Under Frequency 保护功能具有以下可配置的设置:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Disable

Trip Level

90–100% of nominal frequency in step of 1%

94% of nominal frequency

Time Delay

0.1–6000.0 s in step of 0.1 s

0.1 s

Alarm Level

90–100% of nominal frequency in step of 1%

94% of nominal frequency

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.