Markup Information
To display the markup pane, click the Markups button. Be aware that only active markups are displayed. Each markup
record displays its current status, who submitted the markup, the
date it was submitted, and a number of operational choices. From the
markup pane, you can filter markups based on your assigned work, all
available work, markup type, and markup name. You can also assign,
unassign, or complete a markup. For viewing specific markups on the
map, there is functionality that allows you to zoom to a particular
markup and show just that markup in the map.
When more than 50 markups are available, the Markups pane automatically displays only the first 50 records. Click the Load More button at the bottom of the pane to view the next 50 markups. This appends the next 50 markups to the end of the current list. This format allows for a quicker load time when numerous markups are available.
Refresh
Show All Markups
Prior to showing all markups,
click on the Zoom To, Pan To, or Show only this markup button under
any markup record to load the map service into ArcMap. Then, to display
all the markups currently listed, click the Show all markups button
toward the top of the markup pane. The extent does not change, so
you may need to zoom out or pan to see all the markups. Clicking this
button clears out any definition queries that might be applied to
each markup layer.
Select Multiple Markups
You can quickly select multiple markups using either your keyboard or mouse.
Keyboard Select
While holding down the Shift key, as you arrow down, each markup is selected until you let go of the arrow key. If any key is pressed without the Shift key held down, the selected group is no longer active.
Mouse Select
With a markup selected, when you hold down the Shift key and choose another markup, all markups between the first one you clicked and the last one are selected. You can select/deselect a markup by holding down the Ctrl key and clicking the markup. If any key is pressed or mouse button clicked without the Ctrl or the Shift key held down, the selected markups are no longer active as a group.
Show Only This Markup
Filter and Search
-
From the Filter by Assignment drop-down, select the assignment filter you want to apply. From that list, My Work filters by work that’s assigned to you, Available Work shows all unassigned work, Assigned Work displays work that’s assigned to someone, and Current Session lists markups assigned to your current session.
-
Click the All Types drop-down to filter results by markup type.
TIP: The options in your list may look different from what shows in the list above. -
Type in the search field to locate specific markups by name.
-
At this point you can click Assign to Me
if you are going to perform the work. You can also unassign the job or complete it.
Select Markups by Map Selection
Zoom To
Pan To
Assign/Unassign/Complete
The Assign To Me, Unassign, or Complete buttons can be used to change the status of markups. Logged-in users can assign markups to themselves that are either unassigned or assigned to another user. You must have a markup selected in the Markup pane to complete any of these tasks below.
To assign a Markup to yourself, click the Assign To Me button.
To reassign a markup that is currently assigned to someone else, click the Assign To Me button. After a moment, the markup is reassigned.
Once assigned, a markup can be unassigned if it should be returned
to the pool of available markups. To do so, click the Unassign button.
You cannot unassign markups that are not currently assigned to you.
The markup can also be completed by clicking the Complete button.
Select Yes to complete the markup.
If you select No, the markup remains assigned. If you select Yes, the following things happen:
-
The markup is removed from the list.
-
The markup features are removed from the map and the app.
-
A notification is sent to the app that markups have been closed.
Create Session
Click the Create Session button on either a markup that's assigned to you or on an available
markup. This automatically creates a session with that markup assigned
to it. The session automatically opens and pans to the markup when
the version finishes switching. The markup remains associated with
the session until it is completed. When a session is deleted, the
markup is visible in the Markups pane. If it was assigned to you,
it is available in My Work. Otherwise it’s visible in Available
Work.
To create a new session for a markup, the current session must be closed before clicking Create Session.
Photos in Markups
Photos can be added to markups in ArcFM Mobile, which can then be viewed and downloaded from Editor XI.
The camera icon on a markup indicates photos are included with
the markup. Click the Photo button (camera icon) to view a list of
attached photos.
Click the arrow in front of items to display the photo thumbnails.
To view the photo in a separate window outside of the Markups pane, double-click on the photo you want to open.
Click the Zoom button to zoom to and flash the location
of the photo in your map.
The Export button allows you to download the photos to a selected location. Click Export to display the Browse for Folder dialog and navigate to the location you'd like to save the photos. A message displays indicating when the files have been exported. They are exported as individual zip files for each photo that is attached to the markup. Zip files are named according to the photo name displayed in the Markups pane.
Alternatively, you can export photos from the Current Session Filter by Assignment drop-down. In this view, select your Markup, then click the Export button. The attached photos also export as individual zip file.