Create Ducts
Ducts can be added two ways, either in the Duct Layout tab or the Duct List Tab.
If you’re interested in creating a new duct bank and its associated duct bank features, refer to the Create Duct Bank topic for instructions on how to create these features all together.
- To create a duct on a duct bank, right-click inside the duct bank on the Duct Layout tab.
- Input the attributes for the duct you are creating. The
Duct ID can be no more than 20 characters.
The two checkboxes indicate if the duct is Available or already Occupied. These are not mutually exclusive and both boxes can be checked to indicate if a duct is occupied yet still has space available for additional cables.
NOTE: When you add a cable to a duct, the Occupied checkbox automatically checks itself if it is not already checked. - Once you have typed all the duct attributes, click Create.
- Click Save toward the bottom of the Layout Editor pane
to save the new duct to your duct wall configuration. If you click
Cancel, it will remove the duct you just created.
After saving, the NEW and MODIFIED text and associated coloring disappear from the List view and the Duct ID in the Layout view is updated. If there is an associated duct flag, the annotation for the duct flag updates to show the new Duct ID.
Your newly added duct also appears in the ArcGIS Pro map and 3D Scene view.
NOTE: The save button only applies your edits — it does not save the edits in your session.