Tracing Tools

IMPORTANT: Device features are recognized in a trace only when they are sketched on end points of line features. They are not supported when sketched on the edge of a line feature.

In ArcFM Editor XI, the available tracing tools are listed below. The button for each of the Tracing tool palettes is governed by the last selected trace. Editor XI provides the option of showing trace results as selection or as graphics. All traces operate with the assumption a subnetwork controller is upstream from the starting point and is part of a valid subnetwork.

IMPORTANT: Tracing tools only work on a clean subnetwork.

TIP:

The Downstream Protective and Upstream Protective traces select all the protective devices based on the trace chosen.



Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.