Session Manager

Session Manager allows you to create and edit sessions that follow a specific version structure and user roles that have been configured. Session Manager creates an edit session in which an editor can make changes. After the changes are complete, the user sends the session through an approval process. Each session has its own associated version.

Additional workflows are supported as a configuration in Azure. A session (and its associated version) may travel through the process several times before receiving approval and being posted to the geodatabase. The following diagram represents an example workflow.

To access Session Manager, click the Session Manager tab in ArcGIS Pro and the Session Manager toolbar appears.

A flow chart illustrating a sample Session Manager workflow

The workflow an individual session travels is recorded in the session history and is visible on the session card.

The history tab of a session card

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.