Delete Targets

There are two ways targets can be deleted. The first way is to right-click on the target in Targets pane and select Delete.

This removes the target from the Targets pane and from the Esri Create Features pane and the Manage Templates pane.

The second way to delete a target is using the Clear All button on the Targets pane. This deletes all targets present on the Targets pane. It also removes them from the Esri Create Features and the Manage Templates panes.

TIP: Only Esri Templates created by Send to Targets from the map are deleted.

When deleting a target, the Esri Template is not deleted unless it was sent to targets from the map or the Esri Attribute pane.

Once you have removed a target, you can’t undo. A target would have to be recreated from the Attributes pane if needed again.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.