Component Information

The Component Info tool provides you with visual information about network features. This tool is available in Gas, Electric, and Water scenarios. Controllable features, such as switches and breakers, are supported in Electric data sets; Emergency and System valves, along with Regulators, are supported in Gas data sets; and any feature in the Controllable Valve asset group is supported in Water data sets.

For Electric data sets, Component Info supports banks containing one disconnect feature operating on any combination of three phases, or three individual disconnect features each operating on a single phase.

The Disconnect Network category must be applied to any AssetType in the Electric data model so an editor can use Component Info to operate the feature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.